The potential force of the OCP could reshape data centers and networks: the Open Compute Project reports that an Open Compute approach typically leads to 38% greater data center energy efficiency and 24% lower operating costs.
If OCP is a path you’re interested in pursuing, remember that it’s not an all-or-nothing proposition. There are solutions available to help you move in that direction over time and in stages, as your business needs demand it and your budget allows it.
Open Rack Design for OCP
An open bridge rack (OBR), for example, can provide a flexible path that to take you from today’s TIA/EIA-standard rails to open-standard rails when your data center is ready. These racks can be used in three configurations: networking, server and OCP. They allow you to standardize with one rack, no matter the environment.
You can use open bridge racks as standard IT enclosures now. When the migration to Open Compute happens, the racks will be ready – you won’t need to purchase new ones. They convert quickly (in less than 40 minutes) from TIA/EIA rails to Open Compute rails while in the field.
Multi-tenant data centers (MTDCs) also benefit from open bridge racks: They can offer both an Open Compute solution and a standard solution without having to purchase and store double inventory.
The open bridge rack is part of the Open Compute Project’s “grid-to-gates” philosophy, which is a holistic design process that considers the interdependence of everything from the power grid to the gates in the chips on each motherboard.
The Future of OCP
The Open Compute Project began with the hope that the data center community would use the information and lessons shared by Facebook to reimagine, reinvent and make new technology advances. That vision is becoming reality as manufacturers create open-source products for data centers. Separate data center teams, budgets and silos, along with proprietary solutions, are gradually giving way.
To learn more about the Open Compute Project, or how Belden can help you move toward an Open Compute environment, visit our Data Center page.
À propos de l’auteur
Mike Peterson
Responsable Technologie et Applications - Centre de Données
Mike Peterson a rejoint Belden de 2014 à 2016. En tant que responsable de la technologie et des applications, Mike a surveillé les principales activités technologiques du secteur et a gardé un œil sur les tendances émergentes des centres de données. Il a également joué un rôle déterminant dans le développement de relations avec les organismes de normalisation de l’industrie et les alliances commerciales.