Of course, “reliable” is a relative term. Since wired networks have become so reliable and are already trusted, the inevitable gap between wired and wireless can skew perspective and scare some people off from the benefits of wireless technology. And that’s a shame. Truth is, it may never be practical to make wireless fully as reliable as wired connectivity—that’s just physics. But, like wired, wireless is getting better and better, and, with proper planning and equipment, wireless can be an extremely reliable tool perfectly suitable for many, many applications.
In fact, we are seeing wireless deployed more and more in the type of critical applications that may have been considered impossible just a few years ago. Technologies such as strategic use of multiple redundancy mechanisms are bringing these applications well within stringent reliability goal ranges, even for vital safety functions like train control. Here are some other aspects to consider as you work to optimize the reliability of the wireless portions of your networks.

Maximizing Signal Strength
When people say reliability, what they are really talking about for the most part is maintaining the optimum signal to noise ratio, and that means either working to improve the signal or working to reduce the noise, depending on the issues inherent to the particular situation. Often that starts with the proper coverage for the terrain and such issues as antenna selection, with proper placement and installation, as well as studies regarding dead areas or other spots of weak coverage and resulting mediation to remedy them. There are many experts and many products readily available that can help improve signal strength and smooth over most challenges to ensure that you get the coverage you are seeking throughout the target area.
If you are getting good coverage of your signal but still having reliability issues look to the noise side of the signal-to-noise ratio. Interference is a common problem—ensure that there is not a lot of conflicting traffic on the same channel from elsewhere in your organization, such as your IT Department. In many organizations, unfortunately, OT and IT goals operate in silos and you may be inadvertently stepping on each other’s communications quality. Fortunately, once the problem is diagnosed it can usually be readily fixed for everyone. Similarly, we often see issues with interference from the environment. Electrical noise flowing from high voltage equipment like ubiquitous VFDs much less massive ten ton presses are endemic to many industrial environments and that constant or even intermittent barrage is a common culprit in the erosion of signal strength. Professional frequency planning by trained experts is key when setting up a new wireless network to avoid problems down the road, and similar expertise can be engaged to improve conditions in existing networks as well.
In existing networks, among many other custom aspects of your equipment and terrain, the experts will certainly consider the frequency band and IEEE standard that you are utilizing. The 2.4 GHz band was the most common and got very crowded; the emergence of the 5 GHz band eased traffic noise considerably, so a band move and traffic redistribution may be a consideration for many operations. Similarly, the emergence of IEEE 802.11n a few years ago provided a huge boost to wireless reliability, so if your system is utilizing earlier versions 802.11 a, b or g, a change may also be a consideration. In addition, the latest version of the standard, 802.11ac, provides higher data rates and speeds, not only providing significantly better performance, but also, by decreasing transmission times, potentially improving reliability as well.
Look to Security
As noted, there is a wide universe of technology tools than can be applied to most any coverage or capacity challenge. If packet loss cannot be avoided through expert frequency planning, Wireless PRP (Parallel Redundancy Protocol), products can be brought to bear, providing two parallel links per transmission. If you have a mix of older and newer nodes, as many do, the initiation of Airtime Fairness protocols can help optimize the distribution of airtime and increase the performance of the overall network.
When looking to improve reliability, always remember that security is intertwined with it. A move in one can impact the other, so be sure to educate yourself on the impacts of any changes and upgrades. For example, moving up the 802.11 chain (from WEP with legacy IEEE 802.11a/b to WPA2) can not only improve reliability but bolster network security as well, giving you a two-fer and providing even more incentive to retire outdated legacy systems.
The bottom line I believe is that wireless can be both reliable and secure for many, many applications, but getting optimal service doesn’t just happen—it takes knowledge and planning, and making use of both high quality products and high quality expertise. Something that works on paper won’t necessarily work on-site—like discovering IT channel interference on your OT network the hard way. So it pays to avoid underestimating the short term planning that needs to be done to ensure long term reliability, security and performance. Due diligence is the key to getting outstanding results. If you’d like to find out more, we’d welcome a conversation.
À propos de l’auteur
Bernhard Wiegel
Propriétaire du produit
Bernhard Wiegel travaille chez Belden depuis 2012 et est spécialisé dans la communication sans fil et les réseaux. Son rôle actuel chez Belden/Hirschmann se concentre sur le propriétaire du produit sans fil, dirigeant l'équipe de R&D qui développe le produit du portefeuille Wi-Fi et cellulaire Hirschmann. Par le passé, Bernhard a occupé le poste de développeur de logiciels senior et a dirigé le développement du logiciel HiLCOS, qui fonctionne sur la plupart des produits Hirschmann Wireless. Bernhard a obtenu un diplôme d'ingénieur électricien en 2006 et un doctorat en 2013 de l'Université d'Ulm en Allemagne. Au cours de ses activités de recherche à l'Université d'Ulm, il s'est principalement concentré sur la communication sans fil entre les systèmes mobiles et la qualité de service des systèmes de communication intervéhicules.