Graphique 3D de la Terre symbolisant le commerce international, illustration vectorielle.
Mots clés associés

 

Because fiber systems are directional, maintaining polarity is crucial. It defines the direction that optical signals travel inside the fiber. Without polarity, data won’t flow the way it needs to.

 

Ensuring proper polarity means that “transmit” talks to “receive.” In other words, the transmit signal (Tx) at one end of the channel needs to match the corresponding receiver (Rx) at the other end.

 

Many factors impact fiber polarity—and they all have to do with how fiber components interact with one another:

  • General fiber polarity (straight, flipped, crossed, etc.)
  • Pinning (pinned/unpinned), often referred to as gender (male/female)
  • Orientation
  • End-face alignment
  • Pinning
  • Etc.

 

The 3 common types of fiber polarity

In ANSI/TIA-568.3, Optical Fiber Cabling and Components Standard, TIA defines Types of fiber polarity components to be used in Methods of polarity, including:

 

  1. Type A (straight-through): The fiber at position 1 on one side is the fiber at position 1 on the other side.

  2. Type B (inverted): A longitudinal “flip,” where the fiber at position 1 on one side is at the final fiber position (position 12) on the other side.

  3. Type C (twisted-pair): A pair-wise “flip,” where each fiber pair is flipped from one side to the next. For example, the fiber at position 1 on one end arrives at position 2 on the opposing end, while the fiber at position 2 is the fiber at position 1 on the other side.

 

Stop drawing fiber polarity—and start mapping it instead

It’s not uncommon for engineers, designers and installers to use graphics software to “draw” fiber polarity for optical fiber cabling systems. Below is an example of what these drawings look like.

 

null

null

Click the images to expand.

 

These three sketches all represent Type A fiber polarity. Upon first glance, they look different—but they’re actually all the same. The only differentiating factor is the perspective from which the connectors are shown.

 

While drawing tools may make it simple to draw fiber polarity, they also make it too easy to accidentally manipulate drawings incorrectly leading to an error in polarity planning. For example, a vertical flip changes orientation. A horizontal flip changes fiber position numbering. These mistakes make it difficult to reuse drawings or rely on them to make changes.

 

That’s why we’re working closely with TIA to change the way the industry draws or maps fiber polarity. While TIA-TSB-5069, Optical Fiber Channel Polarity, aids in mapping and planning, there’s room for improvement.

 

The goal: to shift the industry toward using visual symbols—very specific types of symbols—instead of drawings. Why? Because symbols convey lots of information in a single glance. (Think about no-smoking signs or pedestrian-crossing signs, for example.) They bring order to how the industry describes, visualizes and models fiber polarity.

 

Within these symbols, we can capture and represent each component’s impact on overall system polarity, including:

  • Connector keyway alignment/orientation, such as mating compatibility, pinning and multi-row optics
  • Fiber position in the connector
  • Strand identifier, such as color
  • Port positioning in frames, modules and cassettes

 

One change we’re suggesting  is the shape of symbols. In TIA-TSB-5069, only round symbols are used. The symbols aren’t intuitive or easy to understand, especially when mapping a complex fiber channel. For example, when symbols are all one shape, you can’t keep track of or differentiate between cables and adapters.

 

For this reason, adapter symbols will be square in shape, while the symbols for cable assemblies will remain round. Inside the shape will be visual information that represents what’s happening inside that cable or adapter.

 

An empty square or circle indicates nothing unusual with the fibers—everything is as you would expect: one goes to one and so on. Directional arrows or squares displayed inside the shapes visually represent what’s happening with the fiber relative to their position in the fiber connectors. 

 

null » src=

null » src=

Cliquez sur les images pour les développer.

 

Avantages de la cartographie de polarité de la fibre

L’utilisation de symboles plutôt que de dessins pour la cartographie de polarité de la fibre offre de nombreux avantages :

  • Au fur et à mesure qu'ils s'étendent (Base-2, Base-8, Base-12, Base-16, etc.), ils sont indépendants de la couleur et des codes de couleur
  • Ils ne sont pas sensibles à la corruption potentielle possible avec les outils de dessin
  • Ils sont faciles à utiliser pour une vérification rapide de la configuration, de la disposition et de la conception
  • Des champs typiques peuvent être ajoutés aux symboles pour représenter des attributs tels que le nombre de brins, la disposition des broches, la longueur, le profil d'atténuation, etc.
  • Ils ajoutent de la profondeur à la conception en permettant d’utiliser des champs spécifiques pour les numéros de pièce, l’objectif, etc.
  • Ils créent un cadre commun qui facilite la documentation et la formation

 

Si vous souhaitez en savoir plus sur la cartographie de la polarité de la fibre à l’aide de symboles et sur ce que cela signifie pour vous, regardez notre webinaire Principes de base de la cartographie de polarité. Deux de nos experts en fibre expliquent soigneusement ces changements à venir, vous guident à travers les nouveaux symboles et décrivent en détail ce que ces changements signifient pour vous et vos projets de fibre.

 

null » src=

Cliquez sur l’image pour la développer.

 

 

Ressources connexes :

À propos de l’auteur

Henry Franc

Ingénieur d'applications de terrain

En mettant l'accent sur la conception, la planification et la construction de centres de données, Henry Franc agit en tant que conseiller de confiance pour des projets de grande envergure ou complexes dans tous les secteurs verticaux, évaluant les besoins commerciaux des clients et trouvant les meilleures options technologiques pour y répondre. Il a également été élu par ses collègues du secteur au poste de vice-président du Comité d'ingénierie des systèmes de câblage de télécommunications TR42.