Communiqué de presse

Belden Expands Focus on Data Center Market with Holistic Solutions from the Rack Space to the Parking Space

Communications de l'entreprise
Belden’s significant investment in its data center offering is reflected with the addition of commercial and support resources, product enhancements, specialized programs and purchase incentives

 

ST. LOUIS--(BUSINESS WIRE)-- Belden Inc. (NYSE: BDC), a leading global supplier of specialty networking solutions, is excited to announce a significant investment in its solution and services offering for the data center market. "This first phase of investment is an enhancement of capabilities, maintaining the focus on the customer. We have already made additions to customer engagement teams such as sales and technical services resources along with collaboration tools such as our soon-to-be-launched Mobile Collaboration Center," explains Vinoo Thomas, Business Director, Strategic Categories. "New product introductions and improved production capacities for data center-specific products are also included in this phase."

Belden's enhancements support the density, scalability, uptime assurance, space-saving, efficiency and ease of use requirements for every type of data center, including enterprise, edge, colocation, hyperscale and containerizeddata centers. The company's holistic data transmission technologies range from cable and connectivity to power and cooling, security, access control, monitoring and more.

Belden has placed a particular focus on the colocation, enterprise and edge data center markets, offering a collaborative approach to working with its customers. Belden data center experts work closely with customers, taking on a partnership approach to design tailored systems that adapt to the customer's specific, mission-critical facility requirements.

Moreover, its solutions for data centers are designed to be used anywhere within white space to grey space, including facilities management and core IT, Ethernet over IP (EoIP) and OT requirements for building controls, command and control, security and surveillance.

Belden’s solution offering for data centers is always evolving to meet and exceed data center demands, specifically within these product lines:

  • The DCX System, which handles the industry’s highest per-square-foot fiber connection density while maximizing signal integrity and usability through a system of optical distribution frame housings, rack-mount solutions, pre-terminated fiber assemblies and cassettes, etc. 
  • Fiber Pre-Terminated Assemblies, including fiber patch cords, hydra patch cords, mass fusion pigtails, MPO trunk assemblies and multi-fiber cable assemblies that offer superior quality and performance

 

"Belden's global footprint ensures that our experts are always available to work alongside your team to learn about your business, understand your processes and design and configure your colocation data centers," says Chrissy Olsen, Global Sales Director, Data Centers at Belden. "'High density' doesn't have to equal 'difficult to manage' and 'lower density' doesn't have to equal 'lower quality.' We ensure that-regardless of size-data centers can have it all."

In addition to investments in new data center solutions and services, Belden will also be introducing its Mobile Collaboration Center, a "data center on wheels," in June 2021. This 43 foot trailer will showcase Belden's large range of fiber optic high density cable and connectivity solutions and services for data center applications. As the program evolves, Belden will also offer several additional data center-specific programs such as partner training and product promotions to support upcoming projects.

To learn more about Belden’s collaborative approach to supporting data centers, visit www.belden.com/markets/data-centers.

Resolving signal transmission needs with IP- and legacy-based solutions that enable a smooth migration to convergence requires a universal approach for enterprise environments. Only Belden's innovative enterprise connectivity solutions take this universal approach. Belden's extensive portfolio spans LAN, data centers, building automation and security and access control to keep information running smoothly. Outstanding global service and support capabilities and application-specific warranty programs complete Belden's unique offering.

À propos de Belden
Belden Inc., a global leader in high-quality, end-to-end signal transmission solutions, delivers a comprehensive product portfolio designed to meet the mission-critical network infrastructure needs of industrial and enterprise markets. Avec des solutions innovantes visant une transmission fiable et sécurisée de quantités toujours plus grandes de données, d'audio et de vidéo, ce qui est nécessaire pour les applications actuelles, Belden se place au centre du passage de l'humanité à un monde connecté. Founded in 1902, the company is headquartered in St. Louis and has manufacturing capabilities in North and South America, Europe and Asia. For more information, visit us at www.belden.com; follow us on Twitter @BeldenInc.

Belden, Belden Sending All The Right Signals, and the Belden logo are trademarks or registered trademarks of Belden Inc. or its affiliated companies in the United States and other jurisdictions. Belden et d'autres institutions peuvent aussi avoir des droits de marque au sens des conditions énoncées dans le présent document.


View source version on businesswire.com: http://www.businesswire.com/news/home/20210413005704/en/

Mary Melchiorre
Responsable Marketing
514-207-6106
Mary.melchiorre@belden.com