Bâtiments intelligents

Créez votre propre manuel de fibre pour concevoir, installer et gérer la fibre &

Henry Franc

Un manuel de fibre n’est pas seulement un guide de pré-planification, mais concerne tout ce qui concerne votre fibre.’ Il définit les exigences du système et les solutions pratiques pour visualiser ce dont vous avez besoin pour réussir.

 


 

As fiber continues to move into the mainstream, managing your fiber projects to achieve the outcomes that you—and your client—expect will be vital. You need to be ready to design, install and manage fiber effectively.

 

And we’ve learned a little trick to make it easier. Want in on the secret?

 

It starts with creating a fiber playbook. There is no single fiber solution that will meet all your needs, which is what makes a fiber playbook so helpful.

 

What’s a fiber project playbook?

Think of a playbook as a roadmap—a diary of trust that spells out how you’ll achieve expected outcomes based on needs and the constraints of your environment.

 

When you build it right, your fiber playbook will empower you to do the following:

  • Capture all the requirements you need to get through your fiber project successfully.

  • Document and ensure that everyone’s goals are met throughout the fiber project.

  • Provide a way to record, formalize, organize and regularly review all the fiber “plays” and strategies your project team can use, along with their impacts.

  • Reduce the amount of time you spend in firefighter mode so you can focus on your job without worrying about as many unexpected emergencies or troubleshooting issues.

  • Develop a framework for succession planning. Even if the playbook won’t be relevant to your role in five or 10 years, it will be very valuable to whoever comes in behind you and needs this information.

 

A fiber playbook isn’t just a guide for the pre-planning phase of design, but for everything involved with your fiber. It helps you lay out system requirements and practical solutions to visualize your target and what you need to achieve success.

 

What information should we include?

At a high level, it should include information about:

  • People
  • Organizations
  • Processes
  • Materials, tools and other technologies

 

It can include pictures, diagrams, examples, and even links for firmware updates and technology resources.

 

Here are some vital components to include in every fiber playbook you create:

 

  • A description of the organization’s needs. What’s driving this need? Why is the need there in the first place? Why must it be addressed? While standards can play a role, you may have to go beyond the standards to achieve what you truly need.

  • The people and organizations that will be impacted. Who will be served by this fiber solution? Who will be involved in the project, and what role will they play? This section should include clients, agents, vendors, channel partners, contractors and consultants.

  • Processes. Record things like workflows, installation practices, trusted resources, formulas, expected performance levels, maintenance tasks and troubleshooting steps.

  • Materials and tools. This section should include documentation of components and equipment, pictures, examples, software and testing gear. Be clear in the language you use so that anyone who picks up the playbook will know exactly which component or piece of equipment you’re referring to.

  • Technologies and other resources. This can involve things like monitoring, security and asset management, as well as the coordination required for these resources.

  • Résultats attendus. Quels résultats attendez-vous ? Comment le succès sera-t-il mesuré et vérifié ? Quelles valeurs de rendement seront priorisées et comment ces valeurs seront-elles documentées ?

 

À quelle fréquence devrions-nous mettre à jour notre manuel stratégique sur la fibre ?

Tout comme le programme de jeu d'une équipe de football change d'une saison à l'autre, le programme de jeu de votre projet de fibre optique changera également en fonction de ce qui se passe avec la technologie, les exigences commerciales, votre environnement et même ce qui se passe dans le monde.’’—’ Il suffit de le demander à tous ceux qui géraient un manuel de projet de fibre lorsque la pandémie a frappé, lorsque l’État du Texas a connu un gel sans précédent ou lorsqu’une tour 5G a été incendiée en Angleterre : des changements seront nécessaires !

 

Par exemple, il y a 20 ans, vous avez peut-être utilisé la fibre OM1 pour connecter des panneaux de commande. Mais, à mesure que les vitesses Ethernet augmentent, la fibre OM1 ne peut pas suivre.’ Votre spécification ou norme interne doit également changer.

 

Prenons l’exemple d’un centre de données. Nous avons travaillé avec un client pour l’aider à mettre à jour son manuel de gestion de la fibre à mesure qu’il modernisait son centre de données. Le manuel comprenait des informations sur la fibre, bien sûr, mais le client ajoutait également des informations sur les nouvelles méthodologies de fin de rangée et sur la façon dont il gère les migrations d’équipements et de technologies.

 

La prochaine étape dans la construction d’un manuel stratégique de la fibre

Alors que le monde entier se connecte via IoT pour prendre en charge l’automatisation et la prise de décision basée sur les données, la technologie de fibre optique adaptative et ciblée sera essentielle pour y parvenir.

 

Une fois que vous aurez identifié ce dont vous avez besoin (et pourquoi vous en avez besoin)—et mieux compris les considérations de conception et de déploiement de la fibre—vous’serez prêt à développer votre propre manuel de fibre.

 

 

 

Ressources connexes :